Welcome to the course list for Renesas Power & Analog product families. Modules from the course groups on this page can be studied individually or taken with others from the catalog as part of a broader learning journey. Remember to check back often as new content will be published regularly!
Get started by selecting a course title below, you will then be re-directed to the Academy registration page. If you are an existing user simply click the 'Sign In' link in the upper right of the screen to login. New users click the 'Register' link in the upper right of the screen and complete a simple one-time registration to create your profile. Once signed in all users can then navigate to the course catalog from the Academy home page, select the Analog & Power course group from the menu and click the 'Take Course' button to launch the session.
If you would like to take a module from this course for a spin beforehand, simply click the Sample Module button below:
Sample Module
Available Memory Product Courses
Introduction to Renesas M1000 & M3000 MRAM - STT Technology
Last Updated
June 18, 2020
In this module, we will introduce the Renesas M3000 and M1000 series, which are high-frequency non-volatile MRAM of 108MHz. Learn how this series of MRAM devices delivers outstanding reliability and over 20 years of data retention performance. Unlike traditional non-volatile SRAM, these devices do not require a backup battery or capacitors. The M3000 supports quad SPI SDR & DDR interfaces, operates from -40 ° C to + 105 ° C, and is available in SOIC or WSON packages. In addition to a description of the target market and application, support documentation is available.
This module will take approx 11 mins to complete.
Back to Courses