Welcome to the course list for Renesas Power & Analog product families. Modules from the course groups on this page can be studied individually or taken with others from the catalog as part of a broader learning journey. Remember to check back often as new content will be published regularly!
Get started by selecting a course title below, you will then be re-directed to the Academy registration page. If you are an existing user simply click the 'Sign In' link in the upper right of the screen to login. New users click the 'Register' link in the upper right of the screen and complete a simple one-time registration to create your profile. Once signed in all users can then navigate to the course catalog from the Academy home page, select the Analog & Power course group from the menu and click the 'Take Course' button to launch the session.
If you would like to take a module from this course for a spin beforehand, simply click the Sample Module button below:
Sample Module
Available Power Product Courses
Renesas ISL81801 & ISL81802 High-Voltage Power Supply Devices
Last Updated
November 02, 2020
PTBP04014: This course introduces Renesas ISL81801, which is the industry's first 80V dynamic bidirectional 4-switch synchronous buck-boost controller with constant voltage and constant current regulation. ISL81802 is the industry's first 80V dual-output/two-phase synchronous step-down controller, with up to 1MHz operation and current sharing capability, suitable for higher power applications. These devices are targeted at 48V telecommunications, data center servers, and rugged industrial applications worldwide.
This course takes about 26 minutes to complete
Renesas ISL9122A Ulra-Low Iq Buck-Boost Converter
Last Updated
October 13, 2020
PTBP04013: This module introduces the Renesas ISL9122A Ulra-Low Iq Buck-Boost Converter. You will learn that this is a flexible buck-boost switching regulator with bypass mode that provides ultra-low quiescent current (IQ) for powering sensors, microcontrollers (MCUs), wireless devices, and other system components. The explosive growth of IoT wireless connectivity applications will be explained and you will be introduced to some practical examples demonstrating some of the key value add features of this device.
This module will take approx. xx minutes to complete
Renesas HIP2210 & HIP2211 100v Half Bridge Drivers
Last Updated
June 24, 2020
In this Academy module you will learn about the new Renesas HIP221x Series of 100V Half Bridge Drivers. You will learn that Renesas pioneered the HIP IC devices in the industry some 25 years ago. This module will take you through the features and benefits the two products now available from this series the HIP2211 & HIP2210. You will also understand the target markets and applications as well as the support tools that will be available for these devices.
This module will take approx. XX minutes to complete.
Introduction to the Smallest 8.2mm Creepage Photocoupler the RV1S92xx&RV1S22xx
Last Updated
December 13, 2019
PTBP04011: In this module we will introduce the world's smallest packaged photocoupler with creepage distance and clearance distance of 8mm class.
These products address priorities of reducing costs, downsizing and efficient use of factory floor space while maintaining compliance with stricter safety standards where longer creepage is required. This module will provide and overview of how the RV1S92xxA and RV1S22xxA solve these problems with the smallest package (LSSO5 / LSSOP) with a creepage distance of 8.2mm.
The learning time is about 13 minutes.
Introduction to RV1S9x60A Family of 15Mbps Photocouplers
Last Updated
July 22, 2019
PTBP04010: The RV1S9x60A is a family of 15 Mbps optocouplers designed to withstand the harsh environments in which industrial equipment is used. This family offers a variety of packages with a minimum footprint with a given strength of isolation and a minimum creepage distance (shortest distance along the package exterior between the two conductors) to ensure safe operation.
This module will take approx 14 mins to complete.
ISL8210/12/80/82M Analog & Digital Power Modules
Last Updated
March 18, 2019
PTBP04009: In this module you will be introduced to the ISL8210M & ISL8212M families of analog and digital power modules.
The material presented will breakdown the key features of these analog-loop Renesas power modules. The course will also cover the ISL8280M & 82M are true Hybrid Digital modules with a PMBus control interface. You will learn about the target applications for these devices as well as the design tool and documentation support that Renesas provides for these products/ This module takes approx 15 minutes to complete.
ISL9241 USB-CTM Buck-Boost Charger
Last Updated
December 05, 2018
PTBP04008: This module introduces the Renesas ISL9241 USB-CTM combo buck-boost charger. In this session you will learn about the key features and benefits of this product. Supporting both NVDC and HPBB configurations the various operational modes of the ISL9241 such as the reverse turbo mode will also be discussed. A selection of target applications will be shown as well as covering
the various modes of operation of the ISL9241 such as HPBB mode and Reverse Turbo mode. This module will take approx. 12 minutes to complete.
RAA210xxx Simple Digital Power Modules
Last Updated
October 10, 2018
PTBP04006: This module will provide and overview of the RAA210 family of digital power modules. It will explain the key benefits and cover the simple configurability and provide some useful resources. This module will take approximately 10 minutes to complete.
High Voltage Buck-Boost Controller Family
Last Updated
October 03, 2018
PTBP04007: This module will cover the key features and benefits of the Renesas 81601 Buck Boost controller. You will learn how this family of products simplifies design, reduces cost and utilizes the latest technologies. This module will take approx. 10 minutes to complete.
Bidirectional Buck-Boost Voltage Regulator
Last Updated
September 01, 2018
PTBP04004: The goal of this module is to provide the learner with a basic understanding of the ISL95338 bidirectional buck-boost voltage regulator, including its features, operation modes, design considerations, and support materials. The training is presented in a single module and is ideal for any designer looking for a quick introduction to the device, those transitioning a USB design to USB Type-C and USB Power Delivery (USB-PD), or those wishing to comply with the USB-PD specification.
Battery Management System Solutions
Last Updated
July 07, 2018
PTBP04002: The goal of this module is to provide the learner with a basic understanding of the ISL94202 and ISL94203 battery management IC solutions. To aid this, it also includes an overview of battery technology and charging design considerations to provide context. This module is ideal for any designer looking for a quick introduction to these devices.
Discrete Power Design vs. Modules
Last Updated
July 01, 2018
PTBP04005: The goal of this module is to provide you with a basic understanding of the challenges presented by discrete power design and how power modules may address some of those challenges. It then provides context with the ISL8203 power module, its features, performance characteristics and available support materials, as well as equipping you to compare cost of both approaches.
The training is presented in a single module and is ideal for any designer looking for a quick introduction to the device.
15A 42V Single-Channel Step-Down Power Module
Last Updated
July 01, 2018
PTBP04003: The goal of this module is to provide the learner with a basic understanding of the ISL8215M 15A 42V single-channel step-down power module, including its features, performance characteristics, design considerations, and support materials.
The training is presented in a single module and is ideal for any designer looking for a quick introduction to the device.
5V, 12V & 40V Switching Regulators
Last Updated
July 01, 2018
PTBP04001: The goal of this module is to provide the learner with a basic understanding of several types of switching regulators, including their features, operation modes, design considerations, and support materials. We’ll cover 40V buck regulators, 12V switching regulators and various low voltage switching regulators. This module and is ideal for any designer looking for a quick introduction to these devices and will take approximately 21 minutes to complete.
Back to Courses