Welcome to the course list for Renesas Interface and Connectivity products. Modules from the course groups on this page can be studied individually or taken with others from the catalog as part of a broader learning journey. Remember to check back often as new content will be published regularly!
Get started by selecting a course title below, you will then be re-directed to the Academy registration page. If you are an existing user simply click the 'Sign In' link in the upper right of the screen to login. New users click the 'Register' link in the upper right of the screen and complete a simple one-time registration to create your profile. Once signed in all users can then navigate to the course catalog from the Academy home page, select the Analog & Power course group from the menu and click the 'Take Course' button to launch the session.
If you would like to take a module from this course for a spin beforehand, simply click the Sample Module button below:
Sample Module
Available Interface & Connectivity
Introduction to Renesas DA1470x Advanced & Highly Integrated Wireless Connection SoC
Last Updated
June 21, 2022
ICBP1000: In this module w introduce the newly launched DA1470x, the flagship product of Renesas' Bluetooth Low Energy product portfolio. This overview will explain the basics of the family, key features, and target applications. The DA1470x is a state-of-the-art wireless SoC family with built-in application processor, 2D graphics processor, voice section detector (VAD), and power management unit (PMU). No other product offers such a high degree of integration in the Bluetooth® LE domain. As a result, customers can enable cost-effective and reliable small form factor designs for complex sensor and graphics processing applications. The study time is about 30 minutes.
Back to Courses