Renesas Webinars
Welcome to Renesas recorded webinar library. Please click on any webinar title to access the link. Should you experience difficulty opening any video
please click here for help.
Remember to check back often as new content will be published regularly!
Available Renesas Product Webinars
Improve Sensor Measurement and Accuracy of Telemetry Data for Satellite Systems
Date Published
February 22, 2021
This webinar will introduce the space community to the newly released ISL73141SEH, which is the first radiation hardened Analog-to-Digital Converter from Renesas. The ISL73141SEH brings to market the highest performance space grade ADC available. This will allow system designers to increase the accuracy of their sensor measurements and improve the accuracy of telemetry data.
适合成本敏感和空间受限应用的入门级低功耗微控制器
Date Published
February 22, 2021
对成本敏感和空间受限应用的需求持续急剧增长,这些应用可以在降低功耗的同时完成更多任务,提供更强性能。服务于消费类设备、工业传感器和医疗保健市场的客户正在努力生产更加小巧、便携的低功耗设计。
在这种市场趋势的背景下,安装在这些应用上的微控制器需要更高的集成度、更低的功耗,并且必须更加紧凑。推动这一进步的关键因素是能效更高的新一代32位单芯片微控制器,例如RA2L1/RA2E1 MCU产品群。
在这场网络研讨会中,我们将提供RA2L1/RA2E1 MCU产品群的完整基础知识。我们将介绍:
主要特性和优势
易于使用的开发环境
适合成本敏感和空间受限应用的解决方案
Blockchain Secured, Endpoint-to-Cloud IoT Management on Renesas RA and RZ
Date Published
February 18, 2021
Large corporations have suffered damaging and expensive losses from cybersecurity attacks through IoT devices. There are many point-solutions for security, but system architects need a complete endpoint-to-cloud solution. Building on the hardware security foundation in Renesas RA MCUs and RZ MPUs, SmartAxiom uses light embedded blockchain technology to deliver such an endpoint-to-cloud solution in a responsive, scalable, and reliable manner. The SmartAxiom solution also eases mass provisioning, reduces operational costs by minimizing the number of keys and certificates, and satisfies the requirements of a Zero Trust environment. Come join our webinar on February 22, 2021 to learn all about it.
Realizing Autonomous Secure IoT Devices with RX MCU Security Solution
Date Published
February 08, 2021
The trend towards digitalization and IoT is progressing rapidly in recent years. As a result, our lives have changed to become more convenient and enriched, but the valuable data and information exchanged are facing security threats.
Implementing autonomous security in each IoT device can counter security threats. With Renesas' RX Security solution, the implementation becomes easier than imagined. Implementing security in the MCU will further strengthen the system security as it is the starting point of the IoT device operation.
Learn about the following information from the webinar:
1. Challenges for achieving security
2. RX MCU security solution based on the hardware security function
3. Partner solution supporting the implementation of security functions using the RX MCU
自律的で安全なIoTデバイスを実現するRX MCUセキュリティソリューション
Date Published
February 08, 2021
近年のデジタル化、IoT化の流れはこれまでにないスピードで進んでいます。これに伴い我々の生活は便利で豊かになっていく一方、そこで使われる価値あるデータ・情報にはセキュリティの脅威が迫ってきています。
この脅威に対抗するためIoTデバイスは自律したセキュリティが必要であり、RX MCUのセキュリティソリューションを活用すればそれを簡単に実現できます。また、IoTデバイスの動作の起点となるMCUを活用したセキュリティの実現は、安全性を強化できます。
本セミナーから、以下の情報が取得できます。
1.セキュリテイ実現に向けた課題
2.課題を解決するRX MCUのハードウエアセキュリティ機能を起点としたセキュリティソリューション
3.RX MCUと連携したセキュリティ機能の実現をサポートするパートナーソリューション
通过RX MCU安全解决方案实现自主安全物联网设备
Date Published
February 08, 2021
近年来,数字化和物联网的趋势正在迅速发展。我们的生活也变得更加便捷和丰富,但是数据的保护和信息的交换却面临安全威胁。
在每个物联网设备中实施自主安全性可以应对安全威胁。借助瑞萨RX安全解决方案,安全性的实施变得比想象中容易。MCU是IoT设备操作的起始点。因此在MCU中实施安全性将进一步增强系统的安全性。
从该网络研讨会中可了解以下信息:
1.如何应对安全的挑战
2.基于硬件安全功能的RX MCU方案解决了所面临的挑战。
3.合作伙伴基于RX MCU安全功能的安全解决方案
Lowest Active Power Consumption and Highest Performance with the RA Family RA4M2 Group
Date Published
February 02, 2021
In this webinar, we will explore the newest member of the RA family. The RA4M2 MCUs offer lowest active power and 100MHz performance simultaneously. This is making the RA4M2 Group ideal for an IoT application platform with a rich variety of different end-products all based on the RA family of microcontrollers.
In addition, we will touch on how you can realize Secure Element Functionality and benefit from better performance, unlimited secure key storage, key management, and lower system cost. We study how to get more out of your MCU design through high integration allowing rich connectivity and endless communication options and up to 512kB of code flash. By using the Flexible Software Package (FSP), we will review a quick and versatile way to build secure connected Internet of Things (IoT) devices.
Entry Line Low Power Microcontroller for Cost-Sensitive and Space-Constrained Applications
Date Published
January 25, 2021
Demand continues to rise dramatically for cost-sensitive and space-constrained applications that do more and perform better while consuming less power. Customers serving consumer devices, industrial sensors, and medical/healthcare markets are striving to produce very low power designs that are smaller and more portable.
In the context of this market trend, microcontrollers mounted on these applications require higher integration, lower power, and must be more compact. The key enablers of such progress are a new generation of 32-bit single chip microcontrollers that are much more power-efficient, such as the RA2L1/RA2E1 MCU groups.
In this webinar, we will provide a complete foundation level understanding of the RA2L1/RA2E1 groups. We will go over:
- Key features and benefits
- The easy-to-use development environment
- Solutions for cost-sensitive and space-constrained applications
省スペース、低コスト化に貢献するルネサスRA ファミリ 新製品エントリーライン 低消費マイクロコントローラ
Date Published
January 25, 2021
開発コストと消費電力を抑えながら、より多くの機能と高い性能を発揮する小型・薄型アプリケーションの需要は年々増加し続けています。コンシューマ機器、IoT/産業用センサー、医療/ヘルスケア分野等の開発設計者は、より小型で低コスト・低消費電力を実現するアプリケーションの開発に努めています。
このような市場動向の中で、これら小型・薄型機器に搭載されるマイクロコントローラも性能を最大限発揮しながら、同時に高集積化・低消費電力化が強く求められています。
ルネサスはこの度高い性能を実現しながら機器の省スペース・低コスト化に貢献する32ビット・シングルチップ・マイクロコントローラRA2L1/RA2E1をリリースしました。このウェビナーでは、RA2L1/RA2E1グループの特長機能とメリットを詳しくご紹介していきます。
How to Create Smartphone-like User Experiences on Renesas' RA6 Family of MCUs (CHINESE SUBTITLES)
Date Published
January 22, 2021
User Experience (UX) is a key differentiator for popular products, especially in the consumer market. Smartphone abundance and their slick interfaces have raised the bar for consumer's UX expectations.
Designing, developing, and deploying a high-quality graphical UX that doesn't adversely impact the profit margin or shelf price is a significant challenge.
If a graphics toolkit could deliver smartphone-like UX, and scale across different product lines (from MCUs to MPUs), manufacturers can drive higher sales and reduce costs.
In this webinar, we will discuss how the Qt graphics toolkit can extract excellent performance from a complete range of embedded hardware, focusing on simple microcontrollers. We will explore how a low-cost chip can substitute a higher-end board without any perceptible impact on the UX, and why this is such a big deal.
How to Create Smartphone-like User Experiences on Renesas' RA6 Family of MCUs (JAPANESE SUBTITLES)
Date Published
January 22, 2021
User Experience (UX) is a key differentiator for popular products, especially in the consumer market. Smartphone abundance and their slick interfaces have raised the bar for consumer's UX expectations.
Designing, developing, and deploying a high-quality graphical UX that doesn't adversely impact the profit margin or shelf price is a significant challenge.
If a graphics toolkit could deliver smartphone-like UX, and scale across different product lines (from MCUs to MPUs), manufacturers can drive higher sales and reduce costs.
In this webinar, we will discuss how the Qt graphics toolkit can extract excellent performance from a complete range of embedded hardware, focusing on simple microcontrollers. We will explore how a low-cost chip can substitute a higher-end board without any perceptible impact on the UX, and why this is such a big deal.
Enabling predictive maintenance & motor control with the Renesas RA6T1 MCU
Date Published
January 13, 2021
Long gone are the days when designing a motor control application was focused on just getting the motor turning. Engineers are now challenged to add additional features on increasingly complex and multifunctional motor control equipment, while reducing time-to-market, minimizing end-product and maintenance costs, and ensuring safe and secure operation of their designs.
One such feature, predictive maintenance based on AI, has become a common requirement for IoT motor control designs because of its ability to enable preemptive corrective actions, reduce maintenance costs, increase asset life, and ensure safety compliance.
In this webinar, we will explore:
• The RA6T1 single-chip MCU optimized for motor control to help lower overall BOM cost
• A full RA6T1 motor solution to easily evaluate and debug motor control applications and reduce development time and effort
• A predictive maintenance solution with AI using the Google TensorFlow™ Lite for Microcontrollers framework to reduce m
RZ A2M TTD JP
Date Published
January 13, 2021
RZ/A2Mは、モバイル機器で広く使われているMIPIカメラインタフェースに対応し、HMI(ヒューマン・マシン・インタフェース)の中でもカメラを使ったアプリケーションに適しています。特に、画像処理向けの大きな特長として、入力画像を高速処理する動的再構成プロセッサ (DRP ; Dynamically Reconfigurable Processor)を搭載しています。DRPはRZシリーズの一部製品に内蔵された特殊なハードウェアであり、従来の組込プロセッサに比べ10倍以上高速な画像処理が実現できるアクセラレータとして、家電から産業機器まで幅広いシステムの画像認識アプリケーションに適用できます。本オンラインセミナーでは、世界で最も低価格でDRPに触れられるMbed™対応ボードであるGR-MANGOと、無償提供するFreeRTOS™ベースのソフトウェアパッケージを用いて、同梱するDRP Libraryを活用したリアルタイム画像処理のご紹介と実際の使用方法をレクチャーします。
モータ制御とモータシステムの予知保全を実現するRA6T1のソリューションのご紹介
Date Published
January 13, 2021
現在、モータ制御機器の設計は、モータを回転させるだけでなく、付加価値を実装するという課題に直面しています。これは、モータ制御機器のスマート化によるものであり、多機能化と低コスト化の両立、開発工数の肥大化、メンテナンスコストの増加といった問題が生じています。
これらの問題を解決する項目として注目されているのが、AIを用いた予知保全機能です。これはメンテナンスコストの軽減、機器の使用期間を延長させ、安全性のコンプライアンスを確保することが可能なため、現在のモータ機器において強く求められています。
このウェビナーでは、下記の内容に終焦点を当てご説明致します。
•モータ機器のBOMコストを削減可能な、モータ制御に最適化したRA6T1シングルチップMCUのご紹介
•モータ制御の評価・デバッグを迅速かつ容易に開始でき、開発期間の短縮に貢献できるRA6T1モータソリューションのご紹介
• メンテナンスコストを削減に貢献できる、Google TensorFlow™ Lite for Microcontrollersフレームワークを使用した、エンドポイントAIによる予知保全ソリューションのご紹介
How to Create Smartphone-like User Experiences on Renesas' RA6 Family of MCUs
Date Published
December 14, 2020
User Experience (UX) is a key differentiator for popular products, especially in the consumer market. Smartphone abundance and their slick interfaces have raised the bar for consumer's UX expectations.
Designing, developing, and deploying a high-quality graphical UX that doesn't adversely impact the profit margin or shelf price is a significant challenge.
If a graphics toolkit could deliver smartphone-like UX, and scale across different product lines (from MCUs to MPUs), manufacturers can drive higher sales and reduce costs.
In this webinar, we will discuss how the Qt graphics toolkit can extract excellent performance from a complete range of embedded hardware, focusing on simple microcontrollers. We will explore how a low-cost chip can substitute a higher-end board without any perceptible impact on the UX, and why this is such a big deal.
1. Welcome Introduction - Andreas Erlebach
Date Published
December 13, 2020
2. EMEA Keynote - Andreas Hammer
Date Published
December 13, 2020
3. Track A -Renesas RA Family Solution - Markus Vomfelde
Date Published
December 13, 2020
3. Track B -Renesas High-end MPU Solutions - Stefano T, Michele B, Stefan U
Date Published
December 13, 2020
4. Track A -Renesas Security Solutions - Kimberly Dinsmore and David Noverraz
Date Published
December 13, 2020
4. Track B -Renesas Power Solutions - Markus M., L'Ubomir F
Date Published
December 13, 2020
5. Tack A - Renesas Capacitive Touch Solutions - Mickael R, Richard W
Date Published
December 13, 2020
5. Track B - Renesas Sensor Solutions - DN, CM, LF
Date Published
December 13, 2020
6. Track A -Renesas Energy Harvesting Solutions - Dirk Genius
Date Published
December 13, 2020
6. Track B - Renesas Motor Control - Suad Jusuf
Date Published
December 13, 2020
How to Access the Sensor with RA MCU (Anna Schroeter)
Date Published
December 10, 2020
Learn about Renesas ARM MCU Solutions (Mickael Haudebourg)
Date Published
December 10, 2020
Live Lab Creation Adding a Simple Emwin GUI and Reading the Sensors (Richard Warner)
Date Published
December 10, 2020
Live Lab Creation Generate, Build, Download and Run ‘RTOS Blinky’ Project (Richard Warner)
Date Published
December 10, 2020
Live Lab Creation: Generate, Build, Download and Run ‘RTOS Blinky’ Project (Richard Warner)
Date Published
December 10, 2020
Live Lab Creation: Use the ZMOD4410 Sensor Together with Air Quality Sensor Kit (Christian Meyer)
Date Published
December 10, 2020
Renesas High-Performance Gas Sensor Solutions – Get the Background and the Theory (Christian Meyer)
Date Published
December 10, 2020
Summary/Q&A/Finish
Date Published
December 10, 2020
Welcome & Introduction (Andreas Erlebach)
Date Published
December 10, 2020
ZMOD Gas Sensor Family: Hardware (Matthias Groening)
Date Published
December 10, 2020
Breakthrough HMI Challenges with the RX MCU Solution
Date Published
December 01, 2020
Introducing Renesas' Human Machine Interface (HMI) solution, improving usability for machine-to-human and human-to-machine connections.
In recent years, it has become increasingly common to operate equipment intuitively, without looking at the manual. The demand for contact-less equipment operations has also increased due to COVID-19 pandemic. The HMI requirements have become more complicated and there is a limit to usability improvement in device operation by using hard keys, the mainstream methodology for embedded devices.
In this webinar, we will introduce technologies such as capactive touch keys, contact-less interfaces, and GUI (Graphical User Interface) that holds the keys to breakthrough the current methodology and improve usability. Renesas will address the challenges and solutions for each technology.
RX MCU解决方案使HMI设计挑战带来突破
Date Published
December 01, 2020
介绍瑞萨人机界面 (HMI) 解决方案,提高人机/机对机连接的可用性。
近年来,直观的界面操作设备越来越普遍,无需查看手册。由于COVID-19大流行,对非接触式设备的需求也增加了。HMI 要求变得更加复杂,使用机械按键(嵌入式设备的主流方法)对设备的操控性改进是有限度。
在此网络研讨会中,我们将介绍诸如触摸按键、非接触式技术和 GUI(图形用户界面)等技术,这些技术是突破当前机械按键方法和提高操控性的关键。瑞萨将针对每种技术提供解决方案。
ユーザビリティのブレークスルーをもたらすRXのHMIソリューション
Date Published
December 01, 2020
機械と人とのコネクションに対するユーザビリティを向上させる、ルネサスのHMI (Human Machine Interface) ソリューションをご紹介します。
近年では、マニュアルを見ずとも直観的に機器操作が出来ることが当たり前となり、またCOVID-19のパンデミックにより非接触での機器操作の需要が高まるなど、HMIに求められる要求がより複雑になってきています。これによって、組込機器では主流となっていたハードキーによる機器操作ではユーザビリティの向上に限界が見えつつあります。
そこで、本オンデマンドセミナーでは、ユーザビリティ向上の鍵となる静電容量タッチキーや非接触インターフェース、GUI (Graphical User Interface) などの技術を紹介し、これらを導入する上での課題に対して、ルネサスが提供するソリューションをご紹介していきます。
Get Your Motor Running in Minutes
Date Published
November 20, 2020
Motor control designers are faced with many challenges including increasing system and power efficiency, enhancing functionality, maintaining, or even increasing the quality grade and accelerating time-to-market. With such demanding requirements, it becomes increasingly difficult to achieve target pricing while accommodating constantly shrinking development schedules.
In this webinar, we will explore an out-of-the-box motor control solution that fulfills a wide range of various application requirements within the 3-phase BLDC, PMSM, and AC induction motor driven applications. You will learn how the BFG motor control solution with the Renesas RA6T1 MCU enables quick and easy evaluation and development of motor control designs while delivering the highest level of quality and performance.
Key benefits include:
Increased system and power efficiency
Design flexibility
Simplified implementation
Enhanced functionality
Faster time-to-market
Decreased system cost
1. Welcome and Introduction (Andreas Erlebach)
Date Published
November 03, 2020
2. Learn about Renesas ARM MCU Solutions (Mickael Haudebourg)
Date Published
November 03, 2020
3. Live Lab Creation - RTOS Blinky, Project, FSP, Sensors (Richard Warner)
Date Published
November 03, 2020
4. Sensoring - PM Sessions (Christian Meyer, Anna Schroeter, Matthias Groening)
Date Published
November 03, 2020
ライバル製品に差をつけろ!RZ/A1H 無償GUIソリューション導入セミナー(オンラインセミナー)
Date Published
October 30, 2020
How to build secure IoT applications with Renesas RA MCUs
Date Published
October 26, 2020
In this webinar, hardware security expert Cesare Garlati will show how to use Renesas e² Studio IDE and Renesas Flexible Software Package FSP to quickly build fully functional secure IoT firmware for the RA Family of 32-bit MCUs. The secure IoT firmware is based on the innovative MultiZone Trusted Execution Environment optimized for Renesas Cortex-M MCUs with Memory Protection Unit PMP or TrustZone. The webinar covers all software and hardware components necessary to build a complete IoT application that securely controls a robotic arm via a cloud MQTT broker. The e² Studio project includes FSP drivers, the Trusted Execution Environment, TCP/IP connectivity, TLS/ECC cryptography, and MQTT client providing telemetry, and OTA applications deployment and remote firmware updates. The secure IoT firmware is built on free and open standards, its open source components are distributed under permissive licensing for commercial use.
通过支持Arm® TrustZone®的Cortex®-M33内核的RA系列MCU,实现安全芯片功能所带来的益处
Date Published
October 26, 2020
In this webinar, we will explore the benefits of Secure Element functionality on your embedded designs using the RA6M4 group with Arm TrustZone in concert with the Secure Crypto Engine.
Integrated Secure Element functionality benefits include:
- better performance
- unlimited secure key storage
- key management
- lower BOM cost
In addition, we will explore how to get more out of your MCU design through high integration which allows rich connectivity and endless communication options, and up to 1MB of code flash with dual bank functionality. By using the Flexible Software Package (FSP), we will review a quick and versatile way to build secure connected Internet of Things (IoT) devices.
クラウド接続に不可欠な セキュアエレメント機能をルネサスRAファミリの 新製品で実現してみる
Date Published
October 20, 2020
機器のIoT化が進む中、セキュリティ対策への意識も高まっています。機器をクラウドに安全に接続するには、鍵や証明書を保管するセキュアエレメントが必要です。しかし、コストや実装面の課題から対策が進んでいないという話もあります。ルネサスの新製品RA6M4マイコンではTrustZoneと独自のセキュリティエンジンにより、そうした課題を解決しています。本ウェビナではその内容を詳しく解説しています。
Renesas Unveils Industry’s Highest Performance 80V Bidirectional Buck-Boost and Dual-Phase Buck DC/DC Controllers
Date Published
October 15, 2020
Renesas as one of the top tier semiconductor manufacturers is releasing its latest power management IC solutions for the emerging 48V architecture in 5G telecom, computing and beyond. ISL81801 is a 80V bi-directional buck-boost controller, while ISL81802 is a dual output / two-phase sync buck controller with a lot exciting features. They both have constant current and constant voltage regulation capability, making them ideal for applications like battery charging, renewable energy, automotive power, and other wide input or wide output industrial applications.
业界性能最为领先,用于48V通讯和数据中心的高压Buck-Boost和双向Buck控制器介绍
Date Published
October 15, 2020
作为国际领先的半导体芯片公司,瑞萨即将推出一系列针对新兴的48伏电信和数据中心应用的电源芯片产品,本次网络会议将分享此系列中最近推出的两颗芯片,ISL81801是80伏,双向buck-boost控制器,ISL81802是80伏,双路输出或两相同步buck控制器,有很多业界首创或领先的性能和参数。ISL81801和ISL81802同时具有恒压和恒流控制功能,使其还适用于电池管理,可再生能源,汽车,与其他宽输入或宽输出的工业应用
Using Ultra-Low Iq Buck-Boost Requlation for Always Connected IoT (CHINESE SUBTITLES)
Date Published
October 08, 2020
The explosive growth of IoT wireless connectivity applications creates a demand for ultra-low power consumption capabilities to drive fast transitions from no load to full load in battery-powered devices. Ultra-low Iq buck-boost regulators are key components for these always connected, low-power IoT devices. This webinar shows examples of design considerations for a variety of ultra-low Iq system designs including wireless earbuds, fitness bands, smart watches, water and gas meters, portable medical devices, as well as battery-powered smart IoT devices.
Using Ultra-Low Iq Buck-Boost Requlation for Always Connected IoT (JAPANESE SUBTITLES)
Date Published
October 08, 2020
The explosive growth of IoT wireless connectivity applications creates a demand for ultra-low power consumption capabilities to drive fast transitions from no load to full load in battery-powered devices. Ultra-low Iq buck-boost regulators are key components for these always connected, low-power IoT devices. This webinar shows examples of design considerations for a variety of ultra-low Iq system designs including wireless earbuds, fitness bands, smart watches, water and gas meters, portable medical devices, as well as battery-powered smart IoT devices.
Realizing the Benefits of Secure Element Functionality with the RA Family of Cortex-M33 MCUs including TrustZone
Date Published
September 30, 2020
In this webinar, we will explore the benefits of Secure Element functionality on your embedded designs using the RA6M4 group with Arm TrustZone in concert with the Secure Crypto Engine.
Integrated Secure Element functionality benefits include:
- better performance
- unlimited secure key storage
- key management
- lower BOM cost
In addition, we will explore how to get more out of your MCU design through high integration which allows rich connectivity and endless communication options, and up to 1MB of code flash with dual bank functionality. By using the Flexible Software Package (FSP), we will review a quick and versatile way to build secure connected Internet of Things (IoT) devices.
WattShareTM Technology Design Considerations (Chinese Subtitles)
Date Published
September 30, 2020
Wireless power sharing or reverse wireless power charging has been prominent in television ads and online promotion, but it’s not just for premium smartphones. See how your wireless power receiver design can change the power flow direction and deliver power to other Qi-certified devices.
In this webinar, Gopi will explain how the WattShareTM feature works, applications of WattShare technology, hardware and software design considerations, and how to prototype your next WattShare design with P9415-R evaluation board.
P9415-R is the world’s first broadly available 15W wireless power receiver with WattShare™ technology, the latest advancement in the Renesas wireless power solutions portfolio. In WattShare mode, the P9415-R delivers up to 5W of power to charge other Qi-certified devices using the same wireless power coil and circuitry to both receive and transmit power wirelessly.
WattShareTM Technology Design Considerations (Japanese Subtitles)
Date Published
September 30, 2020
Wireless power sharing or reverse wireless power charging has been prominent in television ads and online promotion, but it’s not just for premium smartphones. See how your wireless power receiver design can change the power flow direction and deliver power to other Qi-certified devices.
In this webinar, Gopi will explain how the WattShareTM feature works, applications of WattShare technology, hardware and software design considerations, and how to prototype your next WattShare design with P9415-R evaluation board.
P9415-R is the world’s first broadly available 15W wireless power receiver with WattShare™ technology, the latest advancement in the Renesas wireless power solutions portfolio. In WattShare mode, the P9415-R delivers up to 5W of power to charge other Qi-certified devices using the same wireless power coil and circuitry to both receive and transmit power wirelessly.
Realizing the Benefits of Secure Element Functionality with the RA Family of Cortex-M33 MCUs including TrustZone
Date Published
September 23, 2020
In this webinar, we will explore the benefits of Secure Element functionality on your embedded designs using the RA6M4 group with Arm TrustZone in concert with the Secure Crypto Engine.
Integrated Secure Element functionality benefits include:
- better performance
- unlimited secure key storage
- key management
- lower BOM cost
In addition, we will explore how to get more out of your MCU design through high integration which allows rich connectivity and endless communication options, and up to 1MB of code flash with dual bank functionality. By using the Flexible Software Package (FSP), we will review a quick and versatile way to build secure connected Internet of Things (IoT) devices.
TUV認証済み機能安全ソリューション、産業用ドライブ向け機能安全システムをより高いレベルへ
Date Published
September 23, 2020
産業システムに安全と安心をもたらす。
故障時にも安全レベルを維持することを目指す産業分野では「機能安全」の重要性が高まっています。 これは、プラント運転中の故障や事故、オペレーターの負傷、および関連する経済的損失の悪影響を防ぐためです。 欧州連合の安全指令や多くの国の安全関連法では、機能安全基準を満たすための機器が必要です。
ルネサスは、機能安全規格の適用が多くの産業分野に拡大するにつれ、開発期間とお客様の負担を軽減するために、TUVラインランドによる認証済み 機能安全ソリューションと開発ツールを提供しています(IEC61508 )。
このウェビナーでは、最新のルネサス機能安全ソリューションの概要と、産業用ドライブ(ACドライブ、GPインバーター)のアプリケーション例をご覧いただけます。
wolfSSL is RA Ready to Secure Your Device (and 2 Billion More!)
Date Published
September 23, 2020
Please join wolfSSL as they take you through the challenges and successes of securing applications, devices, IoT and the cloud.
Today, security is at the heart of IoT—a web of connected devices and applications. Utilizing wolfSSL’s expertise in securing over 2 billion connections worldwide, the wolfSSL product portfolio offers customers optimal performance, rapid integration, standards compliance, hardware crypto support and Engineering support up to the 24x7 level. wolfSSL takes pride in being the most comprehensively tested and supported cryptography available.
In this session, users will learn how wolfSSL's products are designed for quick and easy integration with an RA Ready project. The integration allows users the ability to leverage hardware crypto solutions, and support for the most current standards. All products are designed for ease-of-use with clean APIs and are backed by a dedicated and responsive support and development team.
符合TUV认证功能安全解决方案将工业传动的功能安全系统提升到更高的标准
Date Published
September 23, 2020
为工业系统带来安全保障。
“功能安全性”在工业领域中变得越来越重要,其目的是即使发生故障也要保持安全水平。 这是为了防止在工厂运行期间发生故障和事故,对操作人员造成伤害以及相关的财务损失的负面影响。 欧盟安全指令和许多国家/地区的安全相关法律要求设备符合功能安全标准。
瑞萨提供了TUV Rheinland认证的功能安全解决方案和开发工具 (IEC61508 ),以减少开发时间并减轻客户负担,因为功能安全标准的应用已扩展到许多行业。
在此网络研讨会中,您将找到瑞萨最新功能安全解决方案的概述以及工业驱动器(交流驱动器,GP逆变器)的应用示例。
Realizing your “Root of Trust” Security into your IoT devices for Tomorrow!
Date Published
September 18, 2020
Please join this unique and latest webinar co-hosted by Renesas and wolfSSL. This session will illustrate how Renesas’s new RX products and Trusted Secure IP (TSIP) can help you implement robust security and how that align with wolfSSL, TLS 1.3 supported embedded SSL/TLS library. In this session, we also show the most recent benchmarking data of wolfSSL comparing that as software implementation versus that is with TSIP hardware acceleration.
Contents:
1. Introducing Renesas RX MCU with dedicated security hardware ‘Trusted Secure IP’ features - By Renesas
2. Experiencing the outstanding security performance of RX MCU with wolfSSL’s SSL/TLS security - By wolfSSL
Raising the Safety Bar in Industrial Drives with TUV Certified Industrial Automation Functional Safety Solutions
Date Published
September 15, 2020
Functional safety in the industrial field is a high priority. This is to prevent the adverse effect of breakdowns and accidents inside plant operation, injuries to operators, and the associated economic losses. The European Union’s Machinery Directive and workplace safety laws, in many countries, require equipment to meet functional safety standards. To reduce the development time and burden on customers, as the application of functional safety standards is extended to many industrial fields, Renesas offers functional safety solutions and development tools certified by TUV Rheinland (IEC61508).
In this webinar, find out more about the latest Renesas Functional Safety Solution overview together with the application example for industrial drives (AC Drive, GP Inverter).
アプリを止めずにデバイス内部を可視化!開発効率upを目指すArm最新開発ツール紹介セミナー(オンラインセミナー)
Date Published
September 09, 2020
アプリを止めずにデバイス内部を可視化できる、新しい開発ツールをご紹介します。
本セミナーでは、ルネサス製品RZ/Tをはじめとする様々なデバイスの組み込みソフトウェア開発に必要な機能を包括的に統合した、新しいArm純正統合開発環境「Arm® Development Studio」についてご紹介します。さらに、システムのふるまいの評価やデバックができる、DTSインサイト社製 RAM計測ツール「EVRICA」を使った動的検証の手法についてご紹介します。デバッグでお困りな方や開発効率upの手法をお探しの方は是非ご覧ください。
一石三鳥
Date Published
September 09, 2020
IoTやインダストリー4.0などの自動化プロセスは、工業生産の未来への鍵です。自動化プロセスを持つアプリケーションを構築するには、M2M通信が必要です。産業用イーサネットプロトコルと呼ばれる標準化された通信プロトコルが全てのデバイスに搭載される事になります。これらのプロトコルは、例えばドイツの"NAMUR"(User Association of Automation Technology in Process Industries)のような標準の要求事項に満たすことができます。
このモジュールによるアプローチは、次の観点でハードウェア開発のみならずプロトコルスタック開発の負担削減に貢献します。
1) ライセンスの費用無しで、複数のプロトコルをサポート
2) 標準的なハードウェア、ソフトウェアインターフェースによりインプリを容易化
3) 認証確認済みプロトコルスタック、サンプルアプリケーション、管理ツールにより開発期間を短縮
R-IN32M3 Moduleは、これらの要件を満たしています。また、ルネサスのASSP製品への移行も容易です。
R-IN32M3 Module並びにソフトウェアパッケージを含むソリューションキット(評価キット)は、お客様に「一石三鳥」のソリューションを提供致します。
一石三鸟
Date Published
September 09, 2020
物联网或工业 4.0 等自动化流程被确定为工业生产未来的关键。构建具有自动化流程的应用需要机器到机器的通信,这将意味着所有未来的设备能够通过工业以太网的标准化协议进行通信。这些协议满足了终端用户组织(如 Namur:德国测量与控制标准委员会)的要求,实现易于调试和设备更换。
使用模块的方法可以将硬件接口和工业以太网协议快速整合并可以实现将开发工作量减少到尽可能低的水平,提供以下产品核心价值i:
1.) 低入门门槛的多协议解决方案和包括协议许可证
2.) 由于是标准硬件和软件接口,易于实现并方便移植
3.) 通过工具、软件包和认证可以实现产品的快速上市
瑞萨 R-IN32M3 工业以太网模块解决方案可以完全满足这些要求。模块硬件配置双端口 RJ45 ,该端口提供顺利移植到瑞萨 ASSP 芯片的途径。借助解决方案套件和相应的软件包,瑞萨 R-IN32M3 模块可以实现“一石三鸟”的解决方案。
バッテリメンテナンス不要のIoTデバイス実現方法
Date Published
September 07, 2020
今後ますます市場が拡大するIoT機器市場ですが、バッテリ充電や交換の手間やコストがかかる、電流供給能力が制限され高機能化することが難しいなど、様々な問題を抱えています。REファミリはEEMBCによって認証された世界トップクラスのエネルギー効率で、超低消費電力と高速動作を両立し、これらの問題を解決します。
本セミナーでは、バッテリメンテナンスレスのIoT機器の実現をサポートする、REファミリの特長、バリュー、評価キット、アプリケーションノートをご紹介します。
高度集成的电池前端简化了36V +电池组的设计
Date Published
September 07, 2020
瑞萨ISL94216通过将所有模拟保护,监视,报告和平衡电路整合到一个设备中,从而解决了36V +电池的集成需求。 这种高度集成的电池前端IC可以实现安全,快速的电池开发,该IC通过集成省去了许多BOM选择和PCB尺寸,并且现在在IC级别上可以解决许多PCB验证和测试难题。
WattShareTM Technology Design Considerations
Date Published
September 04, 2020
Reverse wireless power charging has been prominent in television ads and online promotion, but it’s not just for premium smartphones. See how your wireless power receiver design can change power flow direction and deliver power to other Qi-certified devices.
The P9415-R is the world’s first broadly available 15W wireless power receiver with WattShare™ technology, the latest advancement in the Renesas wireless power solutions portfolio. In WattShare or reverse wireless charging mode, the P9415-R delivers up to 5W of power to charge other Qi-certified devices using the same wireless power coil and circuitry to both receive and transmit power wirelessly. This enables a whole new frontier of wireless charging experiences in smartphones, power banks, and portable industrial and medical equipment. Using P9415-R WattShare technology , powerbanks can include both wireless power receiver and transmitter functions at a low cost.
How to Build IoT Devices without Battery Maintenance
Date Published
September 01, 2020
Although the IoT device market is expected to expand increasingly in the future, there are still various problems faced, such as the time and cost needed to charge and replace batteries and the difficulty in achieving high functionality with limited current supply capacity. Certified by the EEMBC, the RE Family solves these problems as the world's most energy efficient MCU. It combines ultra-low power consumption and high-speed operation features.
In this webinar, we will introduce the features, values, and evaluation kits of the RE Family supporting the implementation of IoT devices without battery maintenance.
Ultra-Low Iq Buck-Boost Requlator for Always Connected IoT
Date Published
August 28, 2020
Ultra-low Iq buck-boost regulators are key components of always connected, low-power IoT devices. This webinar shows examples of design considerations for a buck-boost converter critical for ultra-low Iq designs.
如何将无线充电整合到耳机盒中
Date Published
August 27, 2020
在本次网络研讨会中,我们将探讨推动蓝牙®或真正无线立体声耳机应用增长的市场趋势。以及讨论将Qi标准无线接收器如何整合到耳机充电盒中,这将对消费者和产品设计师提供产品优势。在研讨会中我们也会包含采用无线充电的耳机盒的设计步骤,以便将无线充电功能集成到充电盒中。
Getting Started with C-Trust and IP Protection
Date Published
August 26, 2020
Injecting security into an existing product can be costly and arduous, and the task of protecting your application needs to be solved in a satisfying and uncomplicated way. In this webinar, we will explore how to enable security into your software development flow with just a few steps. Security just moved from a specialist capability into mainstream development! Learn in a practical way how to implement security in your embedded application with C-Trust and Renesas RA devices.
This webinar is for anyone interested in learning about security or needing to implement security in embedded systems.
Getting Started with C-Trust and IP Protection (JAPANESE SUBTITLES)
Date Published
August 26, 2020
Injecting security into an existing product can be costly and arduous, and the task of protecting your application needs to be solved in a satisfying and uncomplicated way. In this webinar, we will explore how to enable security into your software development flow with just a few steps. Security just moved from a specialist capability into mainstream development! Learn in a practical way how to implement security in your embedded application with C-Trust and Renesas RA devices.
This webinar is for anyone interested in learning about security or needing to implement security in embedded systems.
Highly Integrated Front End Simplifies Design for 36V+ Battery Packs
Date Published
August 26, 2020
Renesas ISL94216 solves the integration requirements for 36V+ batteries by bringing all the analog protection, monitoring, reporting and balancing circuits into a single device. Safe, rapid battery development is enabled from this highly integrated battery front end IC, which elminates many BOM selections and PCB size through integration, and many PCB verification and test challenges are now pre-addressed at the IC level.
Three birds with one stone
Date Published
August 26, 2020
Automated processes such as IoT or Industry 4.0 are identified as the keys to the future of the industrial production. A machine to machine communication will be necessary to build applications having automated processes and this will enforce all future devices to be able to communicate through standardized protocols known as Industrial Ethernet Protocols. These protocols fulfill the requirements of End-user organizations like the Namur which is easy commissioning and device replacement.
A module approach is ideal to reduce development effort on the implementation of the Hardware interface, as well as the Industrial Ethernet Protocols to as low as possible, with the following offerings:
1.) Low entry barrier with a multiprotocol solution and all license include
2.) Easy implementation and migration path because standard hardware and software interfaces
3.) Fast time to market with tools, software package and certifications
【第2弾】GR-ROSE(RX65N)で試すSSL/TLSとハードウェア暗号化 --RX65N/TSIPの実力を試してみよう--
Date Published
August 03, 2020
Trusted Secure IP(TSIP)は、ルネサス製RX/RZファミリに搭載されたハードウェア暗号エンジンです。
このセミナーでは、wolfSSL社にて組み込み向けSSL/TLSプロトコルライブラリとRX65NのTSIPハードウェア暗号エンジンを使ったベンチマークを実際に行い、ハードウェア暗号化がもたらす性能改善について紹介します。
本セミナーは第1弾として5/26に開催した「GR-Rose/RX65NでSSL/TLSのクイックスタート(オンラインセミナー)」の続編になります。
Ethernet for Industrial Applications (CHINESE SUBTITLES)
Date Published
August 03, 2020
Long before the birth of Industry 4.0 Ethernet based communication networks had been introduced to the world of Industrial Automation and Process Control applications. With I4.0 the border between the different Ethernet domains are blurring. But what makes Industrial Ethernet so specific, what are the standards used today and why is the new TSN standard so important? This webinar explains the basics.
Ethernet for Industrial Applications (JAPANESE SUBTITLES)
Date Published
August 03, 2020
Long before the birth of Industry 4.0 Ethernet based communication networks had been introduced to the world of Industrial Automation and Process Control applications. With I4.0 the border between the different Ethernet domains are blurring. But what makes Industrial Ethernet so specific, what are the standards used today and why is the new TSN standard so important? This webinar explains the basics.
グラフィカルUIミドルウェア「Aeropoint GUI for RX」組み込み実践 オンラインセミナー
Date Published
August 03, 2020
GUIの開発にお困りですか?「PowerPoint®」で制作しませんか?
「Aeropoint GUI for RX」は、RXマイコンを使った組み込み機器のグラフィカルUI(GUI)の部品配置を、普段から使い慣れた「PowerPoint®」で行うことで、誰にでもGUIの制作を可能にします。
今回、RXマイコンの機能をフルに引き出すこの「Aeropoint GUI for RX」を使い、講師によるリファレンスキットの操作を交えながらGUIの制作・評価をお見せするセミナーです。
How to Integrate Wireless Charging into Earbud Cases?
Date Published
July 27, 2020
How to Conserve Battery Power in IoT Devices (Chinese Subtitles)
Date Published
July 13, 2020
Trends in battery operated IoT devices require increased battery consumption efficiency. This webinar examines cases for consumer and industrial applications where battery life can be extended using different power management techniques.
How to Conserve Battery Power in IoT Devices (Japanese Subtitles)
Date Published
July 13, 2020
Trends in battery operated IoT devices require increased battery consumption efficiency. This webinar examines cases for consumer and industrial applications where battery life can be extended using different power management techniques.
組み込み機器のセキュリティ対策セミナー ~IoTセキュリティ対策の基礎を学びVxWorks®で具体例を理解~
Date Published
July 03, 2020
セキュリティ対策は後付けではなく、設計段階から検討する必要があります。リアルタイムOSを使ったシステムにおいても、セキュリティ対策は免れません。
本セミナーでは、IoTセキュリティの基礎を学びながら、ウインドリバーのリアルタイムOS・VxWorks®によるセキュリティ対策を、デモを交えてご説明します。
Simulating Touch and Analog Layouts with CapExt
Date Published
July 01, 2020
Capacitive touch can be hard. With CapExt we have tried to fix this. In this webinar you will see how CapExt can easily simulate a whole PCB with minimal user interaction in just a few minutes, and how this can be used to make better capacitive touch, saving months of prototyping and possible in-field issues later. CapExt is built for electrical engineers, you only need to provide design files such as Gerbers, and CapExt will handle the rest for you.
Advanced Lasting Data-Retention Endurance Without Battery Back-Up (Japanese Subtitles)
Date Published
June 29, 2020
An MRAM is a non-volatile Magnetoresistive Random-Access Memory. It stores data in a magnetic domain, unlike other RAM that stores in the form of electrical charge or current. Compared to other non-volatile technologies, MRAM excels in applications that require lower power and fast access to back-up data retrieval.
Renesas offers the next generation of MRAM technology with the M1000/M3000 family series. With greater than 20 years of data retention and large memory density, the M1000/M3000 series fills growing non-volatile application needs.
In this webinar, find out how MRAM compares to other memory technologies and key parameters that make it a better choice for your system.
Ethernet for Industrial Applications
Date Published
June 26, 2020
Long before the birth of Industry 4.0 Ethernet based communication networks had been introduced to the world of Industrial Automation and Process Control applications. With I4.0 the border between the different Ethernet domains are blurring. But what makes Industrial Ethernet so specific, what are the standards used today and why is the new TSN standard so important? This webinar explains the basics.
Renesas 5G Sub-6GHz RF solution (CN)
Date Published
June 23, 2020
Renesas has a complete portfolio of RF small signal devices for 5G sub-6GHz applications. While developing new technologies and products to meet changing market requirements, Renesas is committed to the continued support of its established broad product portfolio of standard RF products for our customers. This webinard will provide an overview of recently released products designed to help customer optimize their 5G sub-6GHz system designs with increased performance and reduced costs.
Renesas 5G Sub-6GHz RF solution (EN)
Date Published
June 23, 2020
Renesas has a complete portfolio of RF small signal devices for 5G sub-6GHz applications. While developing new technologies and products to meet changing market requirements, Renesas is committed to the continued support of its established broad product portfolio of standard RF products for our customers. This webinard will provide an overview of recently released products designed to help customer optimize their 5G sub-6GHz system designs with increased performance and reduced costs.
How to Conserve Battery Power in IoT Devices
Date Published
June 19, 2020
Trends in battery operated IoT devices require increased battery consumption efficiency. This webinar examines cases for consumer and industrial applications where battery life can be extended using different power mamangement techniques.
A new era in motor commutation
Date Published
June 18, 2020
Inductive position sensing is changing the game for industrial motor commutation as demands for high performance, high efficiency, and cost efficiency increase, particularly for multi-sector applications.
The IPS2200 is a magnet-free, inductive position sensor IC that can be used for high-speed motor commutation as an absolute position sensor in industrial, medical, and consumer applications.
Stray filed immunity, through-shaft capability, lower weight and smaller size, as well as a substantial BOM optimization make the IPS2200 the ideal alternative for resolver replacement.
In this webinar, you will learn:
-How sensors are used in motor commutation
-The value of inductive position sensors and what problems they solve
-Benefits of using the IPS2200 for motor commutation applications
A new era in motor commutation (CHINESE SUBTITLES)
Date Published
June 18, 2020
Inductive position sensing is changing the game for industrial motor commutation as demands for high performance, high efficiency, and cost efficiency increase, particularly for multi-sector applications.
The IPS2200 is a magnet-free, inductive position sensor IC that can be used for high-speed motor commutation as an absolute position sensor in industrial, medical, and consumer applications.
Stray filed immunity, through-shaft capability, lower weight and smaller size, as well as a substantial BOM optimization make the IPS2200 the ideal alternative for resolver replacement.
In this webinar, you will learn:
-How sensors are used in motor commutation
-The value of inductive position sensors and what problems they solve
-Benefits of using the IPS2200 for motor commutation applications
A new era in motor commutation (JAPANESE SUBTITLES)
Date Published
June 18, 2020
Inductive position sensing is changing the game for industrial motor commutation as demands for high performance, high efficiency, and cost efficiency increase, particularly for multi-sector applications.
The IPS2200 is a magnet-free, inductive position sensor IC that can be used for high-speed motor commutation as an absolute position sensor in industrial, medical, and consumer applications.
Stray filed immunity, through-shaft capability, lower weight and smaller size, as well as a substantial BOM optimization make the IPS2200 the ideal alternative for resolver replacement.
In this webinar, you will learn:
-How sensors are used in motor commutation
-The value of inductive position sensors and what problems they solve
-Benefits of using the IPS2200 for motor commutation applications
GR-Rose/RX65NでSSL/TLSのクイックスタート
Date Published
June 17, 2020
コンパイル環境にe2 studioを使い、wolfSSLとその簡単なサンプルプログラムのソースコードをコンパイル、RX65Nを搭載した評価ボードGR-Roseの上で動作させてみます。自社製品にSSL/TLSあるいは暗号化機能の搭載を検討しているエンジニアの方々に、仕組みと使い方を40分で紹介いたします。
IoT社会を支えるコネクティビティ技術の取り組みとソリューションのご紹介
Date Published
June 16, 2020
エッジからクラウドまでのRXワイヤレス接続の概要。
面向当今物联网社会的瑞萨电子RX无线解决方案
Date Published
June 16, 2020
Securing the Internet of Medical Things with Cypherbridge
Date Published
May 27, 2020
Solving the problem of security in your next IoT design has never been easier with the Cypherbridge SDKPac bundle and Toolkits now integrated and tested on the Renesas RA MCU product line. Cypherbridge design services include product and system integration, and full stack cloud computing. SDKPac is an RA Ready solution to help accelerate time to market, making it easy for customers to securely connect Renesas MCU designs to the internet and for endpoint and edge systems as well.
RX23W Mesh Network Applicable for Smart Home (Chinese Subtitles)
Date Published
May 22, 2020
Bluetooth® Low Energy (BLE) has three main topology options to connect devices. The first option is a point-to-point topology, connecting one-to-one device communication optimized for data transfer and widely used in health management equipment. The second option is a broadcast topology, connecting one-to-many device communications and is ideal for direction searching. The third option is a Mesh topology, connecting many-to-many device communications optimized to control, monitor, and automate multiple systems securely, which is suitable to the current lifestyles that focus on convenience and efficiency.
In our webinar, we are going to deep dive into the Mesh topology data transfer method which will demonstrate integration into a generic system. We will also show how to use the RX23W, the first MCU Group to support full functionality of Bluetooth Low Energy, and its complementary Bluetooth Mesh Software Package to develop a Smart Home with Mesh topology.
スマートホーム向けRX23Wメッシュネットワーク
Date Published
May 22, 2020
Bluetooth®Low Energyには、デバイスを接続するための3つの主要なトポロジオプションがあります。 最初のオプションはポイントツーポイントトポロジで、データ転送用に最適化され、ヘルス管理機器で広く使用されている1対1のデバイス通信を接続します。2番目のオプションはブロードキャストトポロジで、1対多のデバイス通信を接続し、方向検索に最適です。 3番目のオプションはメッシュトポロジで、複数のシステムを安全に制御、監視、自動化するために最適化された多対多のデバイス通信を接続します。これは、利便性と効率性に重点を置く現在のライフスタイルに適しています。 本セミナーでは、一般的なシステムへの統合を示すメッシュトポロジデータ転送方法について詳しく説明します。また、Bluetooth Low Energyの全機能をサポートするRX23Wと、メッシュトポロジを備えたスマートホームを開発するための補完的なBluetooth Meshソフトウェアパッケージの使用方法も示します。
Advanced Lasting Data-Retention Endurance Without Battery Back-Up
Date Published
May 20, 2020
An MRAM is a non-volatile Magnetoresistive Random-Access Memory. It stores data in a magnetic domain, unlike other RAM that stores in the form of electrical charge or current. Compared to other non-volatile technologies, MRAM excels in applications that require lower power and fast access to back-up data retrieval.
Renesas offers the next generation of MRAM technology with the M1000/M3000 family series. With greater than 20 years of data retention and large memory density, the M1000/M3000 series fills growing non-volatile application needs.
In this webinar, find out how MRAM compares to other memory technologies and key parameters that make it a better choice for your system.
Renesas RX Wireless Solution for Today's IOT Society - Introduction to RX Wireless Connectivity from edge to cloud
Date Published
May 20, 2020
In the IoT society such as industrial automation and smart homes, the trend is to collect various information from sensors and other information into the cloud to create new databases. Therefore, wireless connectivity is a very important feature/function for IoT application.
With the technology changing rapidly, there are many challenges and issues in setting up an IoT solution from sensor node to gateway and connects to the cloud. In this webinar, Renesas will introduce ways to reduce the complex product development and shorten development time with RX wireless connectivity solutions and how to overcome the challenges and issues face by most design engineers.
Securing your IP and protecting sensitive data with Renesas MCUs (Chinese Subtitles)
Date Published
May 19, 2020
Functioning as the next webinar in this series, we will give more detailed guidelines and advice on how to protect data on the microcontroller, which is often unchanged, but stored long-term. Different use cases and data types demand varying security implementations. Potential security threats will also have certain influence on security implementation. With this webinar, a developer should be able to make a plan for their own project and implement the mandatory security measures.
Securing your IP and protecting sensitive data with Renesas MCUs (Japanese Subtitles)
Date Published
May 19, 2020
Functioning as the next webinar in this series, we will give more detailed guidelines and advice on how to protect data on the microcontroller, which is often unchanged, but stored long-term. Different use cases and data types demand varying security implementations. Potential security threats will also have certain influence on security implementation. With this webinar, a developer should be able to make a plan for their own project and implement the mandatory security measures.
Automating Machine Learning/AI for RA MCUs with Qeexo AutoML
Date Published
May 08, 2020
In this session, users will learn how Qeexo’s AutoML machine learning platform transforms the embedded AI (Artificial Intelligence) development process without users having to code. Qeexo AutoML is a fully-automated, end-to-end machine learning platform that builds lightweight machine learning solutions (tinyML) running locally on constrained environments such as a Cortex Arm M4 MCU. It augments the user experience and applicability of products like the RA Family of MCUs, adding intelligence with AI for many applications including Wearables, Industrial, Mobile, Smart Home/Appliance and other IoT markets.
HVAC Systems Monitoring Air Quality
Date Published
May 08, 2020
Poor air quality can impact an individual's health and wellness, as well as the global economy. There is currently a lack of sufficient equipment in the consumer market addressing this issue and little expertise on how to design for air quality systems.
We will walk through sensing solutions and technologies that integrate features and capabilities to measure air quality for smart HVAC systems.
In this webinar, we will cover:
-How to define parameters for air quality
-How HVAC systems can be used to monitor and respond to Indoor Air Quality & Outdoor Air Quality changes (ie: detecting gas levels for CO2, TVOC, NOx, O3)
-Design ideas and solutions to help customers get to market faster
Protecting Sensitive Data in Medical IoT Devices
Date Published
May 06, 2020
The Internet of Things (IoT) has facilitated significant advancements in the way healthcare providers deliver care to their patients. As the dependence on connected medical devices such as blood glucose monitors, pulse oximeters, asthma inhalers, and other wearables increases, so does the risk for cyber-attacks and unlawful acquisition of patient data being transmitted through these medical IoT devices. Learn how the RA4W1 provides the security needed to combat these cyber threats in medical IoT devices.
In this webinar we will explore:
• How Bluetooth technology is used in medical IoT devices to
o Help administer medication
o Diagnose injuries
o Transmit critical information securely from patients to providers
• How RA4W1’s Secure Crypto Engine can protect personal data
RX23W Mesh Network Applicable for Smart Home
Date Published
April 28, 2020
Bluetooth® Low Energy (BLE) has three main topology options to connect devices. The first option is a point-to-point topology, connecting one-to-one device communication optimized for data transfer and widely used in health management equipment. The second option is a broadcast topology, connecting one-to-many device communications and is ideal for direction searching. The third option is a Mesh topology, connecting many-to-many device communications optimized to control, monitor, and automate multiple systems securely, which is suitable to the current lifestyles that focus on convenience and efficiency.
In our webinar, we are going to deep dive into the Mesh topology data transfer method which will demonstrate integration into a generic system. We will also show how to use the RX23W, the first MCU Group to support full functionality of Bluetooth Low Energy, and its complementary Bluetooth Mesh Software Package to develop a Smart Home with Mesh topology.
Renesas' Winning Combinations Provide You with Comprehensive Solutions
Date Published
April 24, 2020
Renesas' complementary product portfolios of Analog + Power + Embedded Processing are working together to deliver comprehensive solutions. Our product experts have developed reference designs called "Winning Combinations," compelling product combinations that help our customers accelerate their designs and go to market faster. These Winning Combinations focus on verticals, including industrial, infrastructure, building automation, health/medical and consumer segments to service more customers and partners worldwide.
In this webinar, attendees will learn:
-How Winning Combinations will help customer design challenges
-Where to find the Winning Combinations & what segments they cover
-How to contact Renesas about Winning Combinations
Bringing outstanding real-time performance, network, and HMI to industrial automation equipment
Date Published
April 20, 2020
The latest RX 32-bit microcontrollers - RX72M, RX72N, and RX66N - realize equipment control and network function with a single chip for applications requiring high real-time performance, such as industrial robots, general-purpose inverters, programmable logic controllers (PLCs), and remote I/Os.
Join us in this webinar to find out how the latest RX MCUs bring you outstanding real-time performance, network, and HMI functions with the following key features:
- Industry's fastest on-chip flash memory with read operations at 120MHz
- 4MB on-chip flash memory and 1MB on-chip SRAM, eliminating the need of external memory that slows down the read-speeds
- Single-chip solution to support high-resolution graphics and wired/wireless network due to large on-chip memory
为工业自动化设备带来出色的实时性能,网络连接和人机交互
Date Published
April 20, 2020
最新的RX 32位微控制器RX72M,RX72N和RX66N可通过单个芯片实现设备控制和网络功能,以用于需要高实时性能的应用,例如工业机器人,通用变频器,可编程逻辑控制器(PLC), 和远程I / O。
随着工业自动化设备需要更多的功能和更高的性能,存储容量和读取速度是决定实时性能的关键因素。
参加我们的网络研讨会,了解MCU如何通过以下特点为您带来出色的实时性能,网络和HMI功能。
-业界最快的片上闪存,120MHz读取速度。
-4MB片上闪存和1MB片上SRAM,无需使用外部存储器因而降低读取速度。
-大容量的片上存储器,可支持高分辨率图形和有线/无线网络的单芯片解决方案。
産業オートメーション機器に卓越した
Date Published
April 20, 2020
最新のRX 32ビットマイコンRX72M、RX72N、RX66Nは、産業用ロボット、汎用インバータ、プログラマブルロジックコントローラ(PLC)、リモートI/Oなどの高いリアルタイム性能を必要とするアプリケーションにおいて、機器の制御とネットワーク機能をシングルチップで実現します。
高性能化と多機能化が進む産業オートメーション機器ではマイコンへの性能要求が高まっていますが、マイコンのリアルタイム性能を決める重要な要素として、プログラムを格納するフラッシュメモリの容量と読み出し速度があります。
このウェビナーに参加して、最新のRX72M、RX72N、RX66Nが備えている卓越したリアルタイム性能、ネットワーク、HMI機能についてご確認ください。
- 業界最速クラスの120MHzの読み出し動作が可能な内蔵フラッシュメモリ
- 4MBのフラッシュメモリと1MBのSRAMを内蔵しているため、読み出し速度の遅い外部メモリの接続が不要
- 大容量の内蔵SRAMにより、高解像度グラフィックスと有線/無線ネットワークをシングルチップで実現可能
Security for the Connected World with Renesas MCUs (CHINESE SUBTITLES)
Date Published
April 17, 2020
In today's connected world, security is a hot topic. But what does "security" mean for microcontrollers and the products that incorporate them? Governments and other regulatory bodies are drafting laws and specifications designed to protect consumers, but how does this impact the MCU realm? Please join us for an introduction to the practical application of security concepts, specifically targeted for microcontrollers.
Security for the Connected World with Renesas MCUs (JAPANESE SUBTITLES)
Date Published
April 17, 2020
In today's connected world, security is a hot topic. But what does "security" mean for microcontrollers and the products that incorporate them? Governments and other regulatory bodies are drafting laws and specifications designed to protect consumers, but how does this impact the MCU realm? Please join us for an introduction to the practical application of security concepts, specifically targeted for microcontrollers.
Security for the Connected World with Renesas MCUs (TRADITIONAL CHINESE SUBTITLES)
Date Published
April 17, 2020
In today's connected world, security is a hot topic. But what does "security" mean for microcontrollers and the products that incorporate them? Governments and other regulatory bodies are drafting laws and specifications designed to protect consumers, but how does this impact the MCU realm? Please join us for an introduction to the practical application of security concepts, specifically targeted for microcontrollers.
Security for the Connected World with Renesas MCUs (ENGLISH)
Date Published
April 16, 2020
In today's connected world, security is a hot topic. But what does "security" mean for microcontrollers and the products that incorporate them? Governments and other regulatory bodies are drafting laws and specifications designed to protect consumers, but how does this impact the MCU realm? Please join us for an introduction to the practical application of security concepts, specifically targeted for microcontrollers.
Percepio Device Firmware Monitor
Date Published
April 15, 2020
Personal Medication Adherence
Date Published
April 15, 2020
Personal Medication Adherence (PMA), or lack of PMA compliance, is a $337 billion problem annually in the U.S. that bogs down our healthcare system. Patients forget to take or may confuse their medication, which can result in being readmitted to the hospital, a skilled nursing home or assisted-living facility, or with another visit to the doctor’s office. The advent of the Internet of Things (IoT) has brought various technologies to the forefront that, when applied to PMA devices, can help resolve some of the issues we currently face. The webinar discusses the mandates, opportunities and solutions for Personal Medication Adherence.
Realize truly compact, secure IoT connectivity modules with easy firmware updates
Date Published
April 15, 2020
The explosive growth of the IoT and Industry 4.0 has sparked the need for higher performance, smaller form factor connectivity modules that support the various security aspects required with IoT connectivity—such as confidentiality, data integrity and availability. The RX651 delivers on this need with smaller MCU package sizes that are ideal for compact IoT applications, without compromising performance, The 64-pin RX651 MCUs give customers the small footprint, high performance, and security features they need to safeguard their connected industrial and manufacturing systems against cyber-attacks.
Securing your IP and protecting sensitive data with Renesas MCUs
Date Published
March 27, 2020
As the next webinar of this row we will give more detailed guidelines and advices how to protect data on the microcontroller which is not changed frequently but stored for long time. The different use cases and data types demand different security implementations and also the potential security threads will have certain influence on the security implementation. Based on the webinar a developer should be able to make a plan for his own project and implement the mandatory security ingrediens to realize this plan.
使用宽带毫米波合成器改进高性能射频设计
Date Published
March 11, 2020
使用Renesas的宽带18 GHz毫米波射频合成器改进您的高性能设计。8V97003器件是毫米波和波束形成应用的理想本地振荡器(LO),或高速数据转换器的精密参考时钟。该设备提供了优异的交流性能,改善了系统特性,如在射频应用中的信噪比和EVM,以及在数据转换器应用中的SFDR。
本次网络研讨会探讨:
-在5G和无线电应用中使用8V97003的好处
-关键性能测试结果
-目标应用的好处
-快速成型工具
Improving High Performance RF Designs with Wideband mmWave Synthesizers
Date Published
March 04, 2020
Improve your high performance designs with Renesas' wideband, 18 GHz mmWave RF synthesizer. The 8V97003 device is ideal as a local oscillator (LO) for mmWave and beamforming applications, or a precision reference clock for a high-speed data converter. The device offers excellent AC performance improving system characteristics such as SNR and EVM in radio applications, and SFDR in data converter applications.
This webinar explores: Benefits of using the 8V97003 for 5G and radio applications | Key performance testing results | Benefits for target applications | Tools for rapid prototyping.
PCle Gen5 Webinar
Date Published
March 01, 2020
Renesas PCI Express (PCIe) Timing solutions save product development time and money by implementing “Future-Proofing”. Future-Proofing means designing a device for use over multiple product generations, and it also means maintaining footprint compatibility if next-generation applications need a new device. This webinar explores: the concept of Future-Proofing, the benefits of Future-Proofing and how Renesas implements Future-Proofing for PCI Express timing devices. Register to learn how Renesas PCIe Timing solutions can reduce design time and development costs for your PCIe designs.
Renesas Synergy S5D3 Webinar
Date Published
March 01, 2020
Have you been challenged by your management to design a state-of-the-art IOT solution? Are you searching for the right microcontroller to be used? You don’t want to make any trade-offs, but enjoy large memory, high security, and easy use? The new S5D3 32-bit MCU of the Synergy Platform, combined with the full Renesas Synergy Software package, allows you to start with zero upfront investment. Join the webinar and find out how the new S5D3 can help you.
Simplify Maintenance Failure Detection with e-AI (RX66T) Webinar
Date Published
March 01, 2020
Embedded AI (e-AI) makes motor control more intelligent. In this example, one Renesas MCU realizes motor control and fault detection simultaneously. The e-AI discovers a failure due to an abnormal load condition of the motor. The abnormal load condition is detected by monitoring the current and rotation speed by a so-called inference model representing a trained neuronal network.
ZMOD Webinar
Date Published
March 01, 2020
An outdoor air quality sensor (also known as an OAQ sensor) is a device used to measure the air quality outside of buildings, as it relates to the overall health and wellness of individuals who make contact with outdoor gases. Typical applications include HVAC dampers, smart city infrastructure, heath & wearable's as well as industrial monitoring devices. Renesas offers a line of miniature, digital output and calibrated sensors that detect specific gases that contribute to unhealthy air quality. In addition to indoor air quality and refrigeration air quality, the ZMOD4510 detects ozone (O3) and nitrogen oxide (NOx) contributing to outdoor air pollution. By measuring these gases and using a rating scale to define levels of air quality, these sensors provide vital information that help systems efficiently manage smart air handling systems in buildings, factories, and the home.
RL78 Quick Solutions Webinar
Date Published
February 18, 2020
The RL78 Quick Solutions demonstrate how RL78 low power MCUs combined with Renesas' analog and power products can create high-performance solutions for a wide variety of applications. The RL78 Quick Solutions are easy-to-build reference designs that include a user manual, sample or source code, circuit diagrams, and PCB and BOM information that can help your product development.
RX65N Cloud Kit Webinar
Date Published
February 18, 2020
"Free Technical Webinar: Cloud Connectivity using AWS and the new RX65N Cloud Kit"
* Are you an active user of Amazon FreeRTOS for your MCU designs?
* Are you concerned about support and qualification of FreeRTOS?
* Are you struggling with the challenge of getting your IOT devices to talk to the Cloud?
* Are you having difficulty accessing and understanding the complex Cloud partner requirements?
* Are you concerned over the costs of accessing the Cloud for IOT prototyping?
* Are you looking for an easy-to-use kit that can get your devices connected right away?
Introducing qualification and support of FreeRTOS along with a FreeRTOS-qualified Smart Configurator for RX devices. In addition, we are introducing the new new RX65N Cloud Kit which can simplify the process of getting connected to the cloud using Amazon Web Services (AWS).
The kit comes with everything you'll need to enable fast prototyping of your system and get data sent to the Cloud.
P9222-R for Battery Charging Cases Webinar
Date Published
February 18, 2020
True wireless stereo (TWS) earbuds are getting very popular as more mobile phones eliminate the audio jack. By wearing tiny earbuds, consumers can conveniently listen to music, take phone calls, and avoid getting tangled in their wired headsets. With the small device sizes, it is not practical to charge the tiny earbuds directly so many manufacturers are designing battery cases to both store and charge them. Consumers will benefit from a truly wireless experience when those cases can be charged on any Qi-certified wireless charger or WattshareTM-enabled smartphone. This webinar explores how the features of P9222-R ultra-compact, highly efficient wireless power receiver and how it benefits low-power applications such as battery charging cases.
RZ2AM Dynamic Reconfiguration AI Webinar
Date Published
February 18, 2020
“Technology and hardware suppliers are marching with conviction toward AI with existing architectures and early market solutions, but the journey will be met with challenges and opportunities. OT vendors are at the start of their business transformation, and what they need from their partners is no longer just products and technology. OT vendors are buying into road maps, not chips — buying a journey not a point solution. “(IDC: Embedded Artificial Intelligence: Reconfigurable Processing Accelerates AI in Endpoint Systems for the OT Market).
This webinar will describe Renesas’ Cognitive Solutions portfolio, which is based on designated e-AI engines called DRP (Dynamic Reconfigurable Processor). RZ/A2M embedded MPU with DRP is now available to the broad market, transforming the way AI is implemented in countless industrial applications.
Renesas Synergy S1JA Webinar
Date Published
February 18, 2020
It is essential to select better analog and power devices in a microcontroller system so the system can be efficient from both characteristics and cost standpoints. In this webinar we will review actual designs that use Renesas RL78 microcontroller and analog and power devices and discuss the advantages for the designs.
ISL82xxx Analog & Digital Power Module Family Webinar
Date Published
January 22, 2020
Free Technical Webinar: Benefits and uses of Renesas latest state of the art high performance Power Modules!
Reduce overall design and development time by using Renesas high performance Renesas Power Module solutions.
We can help you improve quality, reliability, and eliminate risks with our latest easy to use Hybrid Digital PMBus family of ultra high density modules.
These Modules use a best in class analog R4TM control loop for unsurpassed input and output transient performance. High density, high efficiency, incredible thermal performance, are combined with superb electrical performance. The end result is all wrapped together in a fully encased, fully complete power train requiring zero design effort other than integration. Versions available are 10A/15A, with and without PMBus, and are all pin-pin compatible allowing system level tweaking as a product progresses through design.
Isolation Device Selection for Industrial Automation
Date Published
January 22, 2020
Industrial Automation equipment such as AC servos, general-purpose inverters and robot controllers, and green energy systems like solar inverters, wind inverters and battery systems require lower power consumption and higher speed communication due to increased data volume needed for control. On the other hand, the noise environment is more severe because the power devices like IGBTs and SiC MOSFETs provide higher speed switching. In addition, it is necessary to meet safety and size requirements. These situations make it difficult to select isolation devices.
This webinar will show the isolation requirements of industrial automation equipment and green energy systems, and introduce the RV1S9x60A from Renesas, which is used for communication between microcontrollers (MCUs) and I/O.
Motor Control Made Easy Webinar
Date Published
January 22, 2020
Reduce design and development time by 2/3 of the given overall development period. Keep the high quality and reliability of your 3-Phase inverter driven Motor Control system. No deadline deliverance extension. Reach the minimum of investments by reducing the overall cost. Enable a faster go-to market design. Sounds good, but is it realistic?
Yes! With the Renesas microcontroller-based 3-Phase Brushless Motor Control Reference Design, you have the unique advantage of using state-of-the-art motor control software combined with flexible hardware, enabling the development of the most advanced brushless 3-phase motor control system. This webinar discusses how easily you can develop 3-phase brushless motor control with the Renesas Motor Control Solutions and reference designs.
Putting Safety features into Battery Management Systems
Date Published
December 03, 2019
In modern Battery Management Systems a large variety of safety features have to be included to provide a safe operation. Renesas’ Li-ion battery pack monitoring, protection and balancing ICs are specifically designed to meet the stringent safety, reliability and performance requirements of portable and battery powered applications such as consumer, industrial & medical products. In this webinar the main safety parameters that need monitoring are discussed as well as how these solution are implemented to provide intelligent battery management systems.
Back to Courses