Welcome to the course list for the RZ MPU family of products. Modules from the course groups on this page can be studied individually or taken with others from the catalog as part of a broader learning journey. Remember to check back often as new content will be published regularly!
Get started by selecting a course title below, you will then be re-directed to the Academy registration page. If you are an existing user simply click the 'Sign In' link in the upper right of the screen to login. New users click the 'Register' link in the upper right of the screen and complete a simple one-time registration to create your profile. Once signed in all users can then navigate to the course catalog from the Academy home page, select the RZ course group from the menu and click the 'Take Course' button to launch the session.
If you would like to take a module from this course for a spin beforehand, simply click the Sample Module button below:
Sample Module
Available RZ MPU Courses
RZ/V2H High End MPU with DRP-AI for AI applications **NEW**
Last Updated
February 29, 2024
ZMBP15010: In this module we introduce the new Renesas RZ/V2H high end MPU for AI Applications. The RZ/V2H is a 32-bit and 64-bit embedded MPU equipped with Renesas' original AI accelerator called "DRP-AI" based on a 64-bit ARM Cortex-A CPU up to 1.8Ghz with low power Embedded AI for Vision-AI applications. You will learn about the product concept and key features of these new devices as well as the target applications that they are suited to.
RZ/G3S MPU Introduction with 5G Connectivity for IOT Gateway Equipment
Last Updated
January 16, 2024
ZMBP15009: In this module we will provide and introduction to the RZ/G3S, the entry-level microprocessors with high CPU processing performance. You will learn about the key features and benefits of these devices, equipped with Arm's latest core Cortex-A55, and with peripheral functions suitable for the development of IOT gateway equipment. We will cover detailed specifications of the RZ/G3S devices, the target markets and applications to which they are suited.
Introduction to Renesas RZ/T2L MPU
Last Updated
March 13, 2023
ZMBP15008: This module introduces the Renesas RZ/T2L group. RZ/T2L is a high-performance MPU realize high-speed,
high-precision real-time control and EtherCAT communication.
EtherCAT communication which are becoming popular in various segments, and application processing can be
realized on a single chip.
Introduction to Renesas RZ/Five MPU
Last Updated
September 19, 2022
ZMBP15007: In this module we introduce the features of RZ/Five with the latest RISC-V AX45MP Single core.
This product group integrates peripheral functions required for developing IoT edge devices into a single chip. In addition, the CPU with improved performance will add value to your system. Study time is about 12 minutes
Introduction to Renesas RZ/T2M MPU for Motor Control
Last Updated
June 03, 2022
ZMBP15006: In this course your will be introduced to the newest device in the RZT series of MPU. The RZ/T2M combines fast and highly precise real-time motor control capabilities and the latest industrial Ethernet on a single-chip, while also supporting functional safety operation. By providing all essential peripheral functions for motor control, the RZ/T2M enables customers to reduce the number of external components, thereby decreasing BOM costs and product size.
Introduction to RZV2L MPU for Vision AI
Last Updated
February 21, 2022
ZMBP15005: In this module provides a high level introduction to the key features of RZ / V2L and RZ / V2M for Vision AI. This presentation will provide the specifications as well as the target applications that these devices are suited for. This module will take approx. 19 minutes to complete.
Introduction to Renesas RZ/G2L & RZ/G2LC MPU
Last Updated
October 26, 2021
ZMBP15004: In this module we will introduce the features of Renesas RZ/G2L and RZ/G2LC with the latest Arm Cortex-A55 core. This product group integrates the peripheral functions required for the development of HMI equipment into a single chip. In addition, the improved CPU adds value to your system. This material provides an overview of the RZ family, product concepts and specifications for the RZ/G2L and RZ/G2LC, and information about the evaluation environment. This module will take approx. 17 minutes to complete.
Introduction to RZ/G2 MPU Solution Platform
Last Updated
February 20, 2019
ZMPB15003: RZ/G2 platform solution addresses the rising needs for higher performance, higher reliability and long term support with maintenance in Industrial and ZMBP15003: In this module we will introduce the RZ/G2 MPU Platform Solution for Industrial and Building Automation. You will learn about the RZ/G2E and M series which correspond to the new generation of ARM 64 bit architecture with latest DDR4 memory that meet the performance requirements of latest industrial equipment. In addition, ECC (Error Check and Correction) function is in place for both internal and external memory that reduce the risk of soft error and raise the reliability performance. Lastly, Renesas’s Linux software package is based on the Civil Infrastructure Platform (CIP) core which has a Super Long Term Support (SLTS) that offers up to 10 years of support, as against the usual 2 years support in the market. This module will take approx. 25 minutes to complete.
Renesas Infrastructure and Online Ecosystem (Module 5)
Last Updated
October 30, 2018
ZMBP14001: This module takes you on a tour of the online services offered by Renesas to make designing with RZ as easy and efficient for you as possible. From video tutorials to engaging in the Renesas engineering forums to collaborate and learn from others, you will learn what you can find and where to find it.
How RZ Solves Target Application Challenges (Module 4)
Last Updated
October 30, 2018
ZMBP15002: This module takes you through a variety of performance-hungry application examples to highlight how you can apply the performance features and high levels of integration found on RZ in the real world.
The RZ Standard Development Environment (Module 3)
Last Updated
October 30, 2018
Please note this module is currently in revision to update content. A new version will be available in Q1 2019.
ZMBP14000: This module introduces the ultimate performance RZ microprocessor family development environment. You will take a guided tour of the hardware tools that let you evaluate, prototype, develop and manufacture. You will also see the wide variety of software support, from IDE's and compilers to code builders and RTOS support.
Detailed Overview of RZ Core Features (Module 2)
Last Updated
October 30, 2018
ZMBP15001: This module provides an in-depth look at the features of the ultimate performance RZ microprocessor family. You will learn about the core and system functions, on-chip memory and peripherals, as well its microcontroller-based design concepts that will make your MPU development easier than ever before.
Introduction to RZ Products & Road-maps (Module 1)
Last Updated
October 30, 2018
ZMBP15000: This module will provide you with a foundation level overview of the ultimate performance RZ microprocessor family. You learn about its key features, get a functional overview of each RZ family group and where they fit, how to develop and where to find support.
Back to Courses