NOTE: Renesas RE family of MCU are no longer being promoted. Modules from this course group are for legacy customer reference purposes only.
Available RE MCU Courses
Renesas RE Family Energy Harvesting system (Module 4)
Last Updated
October 07, 2020
EMBP10005: This course will introduce you to the energy harvesting systems of Renesas RE family. A brief explanation of the energy harvesting system in the RE01 group and the sample program demonstration on the evaluation kit will be explained. It also describes the software design / hardware design for energy harvesting. [Caution] Be sure to watch the training of "Renesas RE Family Development tools settings" and prepare the evaluation environment before taking this course. The required time is about xx minutes.
Renesas RE Family Low power Function (Module 3)
Last Updated
October 07, 2020
EMBP10004: This course describes the low consumption features of the Renesas RE family. The overview of the low power functions, the mode transition, the LPM driver and board settings for current measurement are explained. [Caution] Be sure to watch the training of "Renesas RE Family Development tools settings" and prepare the evaluation environment before taking this course.
The required time is about xx minutes.
How to use the Renesas RE family driver startup and peripheral functions (module 2)
Last Updated
September 29, 2020
This course will show you how to use the drivers (startup, peripherals) of Renesas RE family such as the minimum required settings to operate the RE01 hardware. There are also some specific settings for RE01, so please take this course and make sure the settings.
[Caution] Be sure to watch the training of "Renesas RE Family Development tools settings" and prepare the evaluation environment before taking this course.
Renesas RE Family Development tools Settings (Module 1)
Last Updated
September 24, 2020
This course describes how to set up the development tools for the Renesas RE family. Please take this course first when you start the evaluation because it is explained the required settings to use the RE family.
Renesas RE Family Introduction - The World’s Most Energy Efficient MCU
Last Updated
September 08, 2020
This training introduces Renesas RE Family, a 32-bit MCU product family using Renesas' innovative SOTB™ process technology, and RE01 group. The SOTB™ process technology enables ultra-low current consumption in both active and standby modes and high-speed operation (64 MHz) at a low voltage (1.62 V) that could not be achieved with conventional semiconductor technologies. This low power consumption performance has been certified by getting the world's best score of 705 in EEMBC's ULPMark-CP Benchmark that fairly measures the energy efficiency of MCUs. RE Family provides added value that could not be achieved before to applications such as smart homes/buildings, wearable devices, trackers, structure monitoring, and healthcare by enabling longer battery life, reducing the battery size, and high-speed operation in an environment where the current/voltage supply capacity is limited.
Introduction to Renesas RE Family & RE01 Group
Last Updated
October 31, 2019
EMBP10000: This module introduces the RE Family, the new ASSP product family that uses Renesas' innovative SOTB™ process technology, and the RE01 group, the first group in the RE Family. You will learn that SOTB™ process technology achieves ultra-low consumption of both active and standby current, which was impossible with conventional semiconductors. Also covered is how the use of an energy harvesting controller and a 32-bit CPU enables the development of intelligent energy harvesting IoT devices with maintenance-free batteries. This material is appropriate for anyone evaluating, or wishing to gain and overview of, the RE family and/or the RE01 Group.
This module takes approx.. 15 mins to complete.
Back to Courses
This series of video tutorials will help you to learn the features of Solution, Software and Tools for the Renesas RE family. The Renesas development environment will be introduced in an easy-to-understand manner to help you start your development. Simply click HERE to get started!